Installing new firmware

Turn on the ALC8xxx, while both arrow keys are pressed at the device. 
Now the display shows "display test".

Start a DOS console in the directory which contains both updatealc.exe and the update file.

Invokation:

updatealc firmware.enc -COMx

   firmware.enc : Name of firmware file
   -COMx        : Name of COM port

   Example:
   updatealc updateALC8x00_V1_5.enc -COM3

NOTICE:

The firmware versions for the ALC8xxx and the ALC8xxx-2 are different!
The ALC 8xxx-2 (this version is recognizable from the LEDS on the front panel for the individual channels) needs a diffrent firmware than the ALC 8xxx.

file name for ALC 8xxx   : updateALC8x00_V1_5.enc
file name for ALC 8xxx-2 : updateALC8xxx_2_V1_03.enc

The update procedure lasts approx.. 7 minutes.

Please read in the manual additionally the chapter to the firmware update, in order to install this new firmware.